K65 Ethernet to RS-232 Example Code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K65 Ethernet to RS-232 Example Code

1,557 Views
TerryMcHenry
Contributor II

Customer has been trying examples for the Freescale K65F180M development board from the Kinetis SDK v1.3 and v2.0 using Kinetis Design Studio IDE v3.2. She has had success with the simple USB and serial interface examples, but is still looking for an Ethernet to Serial (RS232) example to pass packets from her computer to the microcontroller and back.  Do you know of any example code for this?

Tags (2)
0 Kudos
Reply
1 Reply

1,419 Views
miduo
NXP Employee
NXP Employee

Please make reference from the thread https://community.freescale.com/message/577390.

Although it is not dedicate for K65, but it should work.

0 Kudos
Reply