Pin Assignment k70 CAN signals

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Pin Assignment k70 CAN signals

1,605件の閲覧回数
chiranjeevn
Contributor III

Hi,

       In my new board i required 2 CAN signals( CAN0 and CAN1). The CAN0 signal i took from  PTB18 and PTB19 whereas for CAN1 i took from PTC16 and PTC17 then i found that PTB16 is shared to NFC_RB signal(NAND Flash).since in my board i m employing NAND flash,GLCD and Xtal pins  i have no other option.Is it ok to connect NFC_RB signal to any GPIO ? Please assist 

ラベル(1)
0 件の賞賛
返信
1 返信

1,523件の閲覧回数
Rick_Li
NXP Employee
NXP Employee

Hi Chiranjeev,

NFC_RB can not be connected to other GPIO, please refer to "K70 signal Multiplexing and pin assignments" section of K70 reference manual.