Pin Assignment k70 CAN signals

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Pin Assignment k70 CAN signals

1,599 Views
chiranjeevn
Contributor III

Hi,

       In my new board i required 2 CAN signals( CAN0 and CAN1). The CAN0 signal i took from  PTB18 and PTB19 whereas for CAN1 i took from PTC16 and PTC17 then i found that PTB16 is shared to NFC_RB signal(NAND Flash).since in my board i m employing NAND flash,GLCD and Xtal pins  i have no other option.Is it ok to connect NFC_RB signal to any GPIO ? Please assist 

Labels (1)
0 Kudos
Reply
1 Reply

1,517 Views
Rick_Li
NXP Employee
NXP Employee

Hi Chiranjeev,

NFC_RB can not be connected to other GPIO, please refer to "K70 signal Multiplexing and pin assignments" section of K70 reference manual.