PFE passive filter

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PFE passive filter

Jump to solution
5,551 Views
jorgevazquez
Contributor II

Hi everyone I´m new using KL25 board and i´m using code warrior and i got a question how does the passive input filter works? in this microcontroller, is filtering high frequencies?or is a band pass filter

I hope you can help me.


Thank you for reading.

Labels (1)
1 Solution
4,672 Views
Paul_Tian
NXP Employee
NXP Employee

This filter is not the traditional filter. It is not high frequencty filter nor band filter. It can looks like a pulse counter. It will delete small width pulse. So it looks like a filter.

View solution in original post

6 Replies
4,672 Views
jorgevazquez
Contributor II

Thanks for your answer, yes it help me to understand this filter thanks for your time

Best regrads.

4,672 Views
Monica
Senior Contributor III

Hello Jorge,

Did that statement help you out?

We'd like to know!

Best regards,

Monica

4,672 Views
FredericoLuiz
Contributor II

Hello Monica Arvizu,

I searched for more detailed information about this Passive Filter but I didn't find  helpful information. The only thing I saw is:

"These pins have a passive filter enabled on the inputs. This is the shortest pulse width that is guaranteed to be recognized."

But I would like to know more about this filter, maybe they could improve my application for reading a keyboard. I'm using a KL05Z32.

Thanks,

Frederico

0 Kudos
Reply
4,673 Views
Paul_Tian
NXP Employee
NXP Employee

This filter is not the traditional filter. It is not high frequencty filter nor band filter. It can looks like a pulse counter. It will delete small width pulse. So it looks like a filter.

4,672 Views
hajianik
Senior Contributor I

Does it replace software debounce?

0 Kudos
Reply
4,672 Views
kora
Contributor II

Is there any more detailed information on the passive filters for GPIO Pins to be found somewhere.

I'm using a Kinetis K64F and have looked through the available Reference Manual and Datasheet but detailed information about this functionality is very sparse?

0 Kudos
Reply