Optimal clock settings for external resonator

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Optimal clock settings for external resonator

1,995 次查看
zainali
Contributor II

Hi,

I trying to find the optimal settings for system oscillator. I am using external clock source with 8Mhz resonator. The oscillator configuration in reference manual shows 3 modes,

zainali_0-1637328036745.png

Can anyone guide what configuration should i choose as 8 Mhz is overlapped. Also is gain linked to the accuracy?

The Microcontroller i am using is MK10DN512 and schematic of oscillator can be seen below.

zainali_1-1637328756166.png

 

Thanks

标签 (1)
0 项奖励
回复
2 回复数

1,988 次查看
bobpaddock
Senior Contributor III

High Gain Mode 2 would be the most reliable.

Gain is more linked to power consumption and start time than accuracy.
Accuracy is determined mostly by the grade of the resonator.

I can't speak to this particular chip, however I've seen reliability problems over the years with using low power (low gain) oscillators.  They don't always start reliably across voltages and temperature ranges.

If your resonator has internal caps, disable any built-in caps that the chip may offer.

0 项奖励
回复

1,980 次查看
zainali
Contributor II

@bobpaddock  thanks for valuable information.


For sake of knowledge, is there any reason to go with high gain mode 2.

Thanks again

 

0 项奖励
回复