Optimal clock settings for external resonator

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Optimal clock settings for external resonator

1,941 Views
zainali
Contributor II

Hi,

I trying to find the optimal settings for system oscillator. I am using external clock source with 8Mhz resonator. The oscillator configuration in reference manual shows 3 modes,

zainali_0-1637328036745.pngzainali_0-1637328036745.png

Can anyone guide what configuration should i choose as 8 Mhz is overlapped. Also is gain linked to the accuracy?

The Microcontroller i am using is MK10DN512 and schematic of oscillator can be seen below.

zainali_1-1637328756166.pngzainali_1-1637328756166.png

 

Thanks

Labels (1)
0 Kudos
Reply
2 Replies

1,934 Views
bobpaddock
Senior Contributor IV

High Gain Mode 2 would be the most reliable.

Gain is more linked to power consumption and start time than accuracy.
Accuracy is determined mostly by the grade of the resonator.

I can't speak to this particular chip, however I've seen reliability problems over the years with using low power (low gain) oscillators.  They don't always start reliably across voltages and temperature ranges.

If your resonator has internal caps, disable any built-in caps that the chip may offer.

0 Kudos
Reply

1,926 Views
zainali
Contributor II

@bobpaddock  thanks for valuable information.


For sake of knowledge, is there any reason to go with high gain mode 2.

Thanks again

 

0 Kudos
Reply