OpenSDA, UART

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,984件の閲覧回数
steffenwickersh
Contributor I

Hello There,


I have another question. It is possible to flash the MCU on FRDM KL03Z motherboard via UART ?


I have five lines to the target MCU measured with my scope . Currently, only the reset line and SWD_CLK SWD_DIO be used..

Thanks!

0 件の賞賛
返信
1 解決策
1,777件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Steffen Wichersheim,

      Yes, you can use UART to flash the KL03 MCU, because this chip have the kinetis ROM bootloader.

    For details, please refer to the Chapter 11 Kinetis ROM Bootloader in  the KL03 reference manual.

Wish it helps you!


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,778件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Steffen Wichersheim,

      Yes, you can use UART to flash the KL03 MCU, because this chip have the kinetis ROM bootloader.

    For details, please refer to the Chapter 11 Kinetis ROM Bootloader in  the KL03 reference manual.

Wish it helps you!


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信