OTAP about hrs by example on KW36

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OTAP about hrs by example on KW36

ソリューションへジャンプ
2,073件の閲覧回数
yeyue
Contributor II

hi ,

I use kw36 board and sdk2.2.9 while using example as zipped in "AN12775SW.zip" download from nxp websit,which is an example about hrsotap, but after finish building, when doing debug, it give out "Thread #1 57005 (Suspended : Signal : SIGTRAP:Trace/breakpoint trap) 0xdeadbeee" ,which means 

Failed to execute MI command:
-data-disassemble -s 3735928558 -e 3735928698 -- 3
Error message from debugger back end:
Cannot access memory at address 0xdeadbeee

and according to "https://www.nxp.com.cn/docs/en/application-note/AN12775.pdf" 

I change to sdk2.2.2 ,it gives out the same error when debugging.

so I need your helps how to solve this.

@EdgarLomeli  @anyone who can give helps

thanks

0 件の賞賛
返信
1 解決策
2,066件の閲覧回数
yeyue
Contributor II

solved.because the bootloader has been modified by other man,so after change the bootloader back to "bootloader_otap_frdmkw36.bin",it works

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,067件の閲覧回数
yeyue
Contributor II

solved.because the bootloader has been modified by other man,so after change the bootloader back to "bootloader_otap_frdmkw36.bin",it works

0 件の賞賛
返信