OTAP about hrs by example on KW36

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OTAP about hrs by example on KW36

Jump to solution
2,082 Views
yeyue
Contributor II

hi ,

I use kw36 board and sdk2.2.9 while using example as zipped in "AN12775SW.zip" download from nxp websit,which is an example about hrsotap, but after finish building, when doing debug, it give out "Thread #1 57005 (Suspended : Signal : SIGTRAP:Trace/breakpoint trap) 0xdeadbeee" ,which means 

Failed to execute MI command:
-data-disassemble -s 3735928558 -e 3735928698 -- 3
Error message from debugger back end:
Cannot access memory at address 0xdeadbeee

and according to "https://www.nxp.com.cn/docs/en/application-note/AN12775.pdf" 

I change to sdk2.2.2 ,it gives out the same error when debugging.

so I need your helps how to solve this.

@EdgarLomeli  @anyone who can give helps

thanks

0 Kudos
Reply
1 Solution
2,075 Views
yeyue
Contributor II

solved.because the bootloader has been modified by other man,so after change the bootloader back to "bootloader_otap_frdmkw36.bin",it works

View solution in original post

0 Kudos
Reply
1 Reply
2,076 Views
yeyue
Contributor II

solved.because the bootloader has been modified by other man,so after change the bootloader back to "bootloader_otap_frdmkw36.bin",it works

0 Kudos
Reply