OS Time Change in SleepMode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

OS Time Change in SleepMode

2,008 次查看
somesh_malla
Contributor II

Hi,

In my project we configured different frequencies as below for MK20FX512VMD12

  • Y1 = 16 MHz crystal oscillator
  • Load capacitance set by OSA0_CR registers = 10 pF
  • Clock input is selected to EXTAL0 (16MHz)
  • PLL pre-divider = 2, multiplier = 30
  • OUTDIV1 = 0 OUTDIV2 = 1 OUTDIV3 = 2   OUTDIV4 = 5

Module Clocks

  • PLL = 240 MHz (16 MHz / 2 * 30)
  • MCGOUTCLK = PLL / 2 = 120 MHz
  • Core Clock = MCGOUTCLK / OUTDIV1 (0) = 120 MHz
  • Bus Clock = MCGOUTCLK / OUTDIV2 (1) = 60 MHz
  • FlexBus Clock = MCGOUTCLK / OUTDIV3 (2) = 40 MHz
  • SRAM Clock = MCGOUTCLK / OUTDIV4 (5) = 20 MHz

MCG_C1 0x20 (External reference clock is selected)

Enabled the sleep mode by setting the LPTMR TEN and TIE bits of LPTMR register

Low Leakage Stop Mode in SMC_PMCTRL register

SLEEPEEP bit in System Control Register

After WFI instruction it waits for interrupt, after this point what is the system/core clock frequency?

As it was configured to use external reference clock in low power mode can I consider 16MHz as the clock used as System/Core clock during this sleep mode?

But from the reference manual it is given as System/Core clock will become divide by 8, which is correct? does it uses external reference clock or it divides the frequency by 8 for computation?

Please see https://community.nxp.com/t5/Kinetis-Microcontrollers/OS-Time-Change-after-coming-out-from-SleepMode... for more details.

 

Regards,

Venkata

0 项奖励
回复
2 回复数

1,991 次查看
danielchen
NXP TechSupport
NXP TechSupport

Hi @somesh_malla :

 

The RTOS tick is the operating system time unit. RTOS measures time in ticks, instead of in seconds and milliseconds.   Which RTOS you are using?  FreeRTOS or MQX RTOS?

 

Regards

Daniel

标记 (1)
0 项奖励
回复

1,982 次查看
somesh_malla
Contributor II

Hi Daniel,

We are using Micrium RTOS, Also attached the register settings read in normal mode and low power mode.

 Normal ModeLow Power ModeNormal ModeLow Power Mode
MCG_C10010000000001110FRDIV=16
External reference clock is selected.
FRDIV=2
Slow Internal Reference clock is selected
Internal Reference Clock Enable
Internal Reference Stop Enable
MCG_C21001010000000111High frequency range selected for the crystal oscillator
FLL or PLL is not disabled in bypass modes
Slow internal reference clock selected.
Low frequency range selected for the crystal oscillator
FLL or PLL is disabled in bypass modes (lower power)
Fast internal reference clock selected
MCG_C50000000110000000Selects OSC0 clock source as its external reference clock
PRDIV0 = 2
Selects OSC1 clock source as its external reference clock
PRDIV0 = 1
MCG_S0110111000000111PLL0 has acquired lock.
Source of PLLS clock is PLLCS output clock
Output of the PLL is selected
Source of internal reference clock is the slow clock (32 kHz IRC).
Source of PLLS clock is FLL clock
Internal reference clock is selected.
Source of internal reference clock is the fast clock (4 MHz IRC).

Regards,

Somesh

标记 (1)
0 项奖励
回复