No Disable Option for some IO's

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

No Disable Option for some IO's

1,141 Views
razumovskyeduar
Contributor I

Hi

Can specific IO can be configured as "DISABLED" if there is no option like this in it's datasheet ?

For example G8:

pastedImage_1.png

If not - what is the preffered configuration for savig power (input PD/PU, Output) ?

Another thing - If pin configured as "DISABLED", it is enough for saving power ? or more configurations should be done (PD,PU) ?

Thanks

Edi

0 Kudos
Reply
1 Reply

1,089 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

For the G8 pin default function is analog input pin, it could be left floating.

The digital IO pin with default "DISABLE"  will saving the power. There does not need to configure related pin, keep default "Disable" setting.


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply