New Kinetis Kxx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

New Kinetis Kxx

2,001 Views
Microfelix
Contributor IV

Hi,

are many years that the use of micro freescale and in particular, the K22, K60 and K70.

Now my needs have grown, and would have the need to use a FLASH bigger.

The current micro stop to 1Mb.

Whereas it was studying a new core M7, the latter will be used for a new family Kinetis?

It will come out with a larger capacity (2Mb)?

Thank You

Maurizio Felicioni

0 Kudos
Reply
3 Replies

1,787 Views
LuisCasado
NXP Employee
NXP Employee

Hi Maurizio,

The answer is yes. But you need contact with local marketing/sales people as the information is under NDA.

Best Regards,

Luis

0 Kudos
Reply

1,787 Views
Microfelix
Contributor IV

dear luis,

to thank you for the answer.

I contacted my local marketing/sales, but still no answer.

Could you be kind enough to tell me what models of Kinetis are there?

Maurizio

0 Kudos
Reply

1,787 Views
mjbcswitzerland
Specialist V

Hi

I have seen that the 240MHz KV5x Cortex-M7 parts have been added to the product page (pre-production):

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=KV5x

Since Atmel (SAMx7) and ST-Micro (STM32F7xx) are now being launched and are included as parts in IAR's latest workbench things must be hotting up!!!!

Regards

Mark

Kinetis: µTasker Kinetis support

For the complete "out-of-the-box" Kinetis experience and faster time to market

0 Kudos
Reply