New Freedom FRDM-K64F board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

New Freedom FRDM-K64F board

1,636件の閲覧回数
mjbcswitzerland
Specialist V

Hi All

The new Freedome board was unveiled today at FTF Americas. Costing about $29 it is packed full of features:

  • Freescale K64F Kinetis K64 MCU (MK64FN1M0VLL12)
    • High performance ARM® Cortex™-M4 Core
    • 120MHz, 256KB RAM, 1MB FLASH
    • SPI (3)
    • I2C (3)
    • UART (6)
    • USB OTG / Host / Device
    • USB
    • PWM
    • ADC (2x 16bit with mux)
    • DAC (2x 12bit)
    • Touch Sensor
    • GPIO

FRDM-K64F Onboard Additions

  • FXOS8700CQ - 3-axis accelerometer and magnetometer
  • Ethernet
  • 2 push buttons
  • RGB LED

Full details are at FRDM-K64F: Freescale Freedom Development Platform for Kinetis K64, K63, and K24 MCUs

The uTasker proejct has been ported to this new board and a simulation is already available as discussed here: New Freedom FRDM-K64F board

Regards

Mark

ラベル(3)
タグ(2)
0 件の賞賛
返信
0 返答(返信)