Need help with the SPI in Expert Mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need help with the SPI in Expert Mode

2,004 Views
roytrapp
Contributor I

Hello at everyone!

Can someone tell me, what i have to do, to initialize the SPI at the main.png (see below) ?

Thanks,

Roy

0 Kudos
Reply
3 Replies

1,890 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Roy,

   Please check the attached SPI PE project, it is the CW project for KL25.

   You can refer to this project add the SPI PE module, then add the according code.

   Wish it helps you!


Have a great day,
Kerry

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,890 Views
roytrapp
Contributor I

Hello Kerry.

Thank you for your help.

What means CW?

And where is the attatched project?

Thanks,

Roy

0 Kudos
Reply

1,890 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Roy,

  CW is the codewarrior IDE.

  About the project, you can refer to the official KL25 CW project:

https://www.nxp.com/downloads/en/lab-test-software/KL25_SC.exe 

The project folder:kl25_sc_rev10\klxx-sc-pex\projects\spi_demo

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply