Need help with the SPI in Expert Mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Need help with the SPI in Expert Mode

2,010件の閲覧回数
roytrapp
Contributor I

Hello at everyone!

Can someone tell me, what i have to do, to initialize the SPI at the main.png (see below) ?

Thanks,

Roy

0 件の賞賛
返信
3 返答(返信)

1,896件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Roy,

   Please check the attached SPI PE project, it is the CW project for KL25.

   You can refer to this project add the SPI PE module, then add the according code.

   Wish it helps you!


Have a great day,
Kerry

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,896件の閲覧回数
roytrapp
Contributor I

Hello Kerry.

Thank you for your help.

What means CW?

And where is the attatched project?

Thanks,

Roy

0 件の賞賛
返信

1,896件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Roy,

  CW is the codewarrior IDE.

  About the project, you can refer to the official KL25 CW project:

https://www.nxp.com/downloads/en/lab-test-software/KL25_SC.exe 

The project folder:kl25_sc_rev10\klxx-sc-pex\projects\spi_demo

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信