NXP FRDM KW35/36 : HCI loopback possible or not?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXP FRDM KW35/36 : HCI loopback possible or not?

2,661件の閲覧回数
skalyan2
Contributor IV

Hi, Is HCI loopback possible with KW35/36 ? if yes, can you please share the procedure ?

4 返答(返信)

2,436件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Sai,

Please look at the HCI_Read_Loopback_Mode command.

For a better reference, Look at the Bluetooth LE Specification.

pastedImage_1.png

Regards,

Mario

2,436件の閲覧回数
skalyan2
Contributor IV

Hi Mario,

Greetings for the day!

Many thanks for your instant reply, I tried sending HCI_Read_Loopback_Mode in KW36 by using the following procedure : 

1) Flashed the HCI_BB in KW36.

2) Opened test tool and tried sending HCI_Read_Loopback_Mode.

I receive the return parameter as Unknown_HCI_Command_Error.

HCI_Read_Loopback_Mode_error.PNG

What i need to know is that, IS HCI_Read_Loopback_Mode/ HCI_Write_Loopback_Mode possible with KW36 ? 

Many thanks in advance!

Regards

Sai Kalyan

0 件の賞賛
返信

2,436件の閲覧回数
xing_chang
NXP Employee
NXP Employee

Hi [email protected]‌,

These commands should not be supported, I will confirm with R&D further, and will reply to you as soon as I have the results.

2,436件の閲覧回数
xing_chang
NXP Employee
NXP Employee

I see the following explanation in the BT core spec, maybe, this does not apply to Bluetooth LE, it is just the BR/EDR command.

This command writes the value for the setting of the BR/EDR Controller’s Loopback