NMI_B not beeing inserted on KL03Z

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NMI_B not beeing inserted on KL03Z

2,677件の閲覧回数
tomazlov
Contributor II

I have Kinetis MKL03Z8VFG4 on custom board and trying to setup NMI interrupt handler to handle logic 0 during the boot (i.e. external device is connected to pin PTB5/IRQ_12/NMI_b  and pulling to GND). I have setup MWE from SDK 2.x example where FOPT register is beeing set:

__attribute__ ((used,section(".FlashConfig"))) const struct {
   unsigned int word1;
   unsigned int word2;
   unsigned int word3;
   unsigned int word4;
} Flash_Config = {0xFFFFFFFF, 0xFFFFFFFF, 0xFFFFFFFF, 0xFFFF3FFE};

Looking into datasheet my configuration sets:

  • BOOTSRC_SEL = 00 (Boot from FLASH),
  • FAST_INIT = 1 (Fast Initialization),
  • RESET_PIN_CFG = 1 (RESET_b pin is dedicated),
  • NMI_DIS = 1 (NMI_b pin/interrupts reset default to enabled),
  • BOOTPIN_OPT = 1 ( Boot source configured by FOPT[7:6] ( BOOTSRC_SEL) bits),
  • LPBOOT = 11 (Core and system clock divider (OUTDIV1) is 0x0).

Then I override default WEAK IRQ handler by defining:

void NMI_Handler(void)
{
   LED_RED_ON();

   delayMS(1000);

   // TODO: handle NMI_b pin state
}

..but PC never goes into this function.

Why is NMI_Handler(void) not beeing called, I am missing something?

ラベル(1)
3 返答(返信)

2,486件の閲覧回数
mjbcswitzerland
Specialist V

Hi

NMI_DIS = 1 (NMI_b pin/interrupts reset default to enabled),

is incorrect. A '1' disables the NMI and doesn't enable it.

Regards


Mark


Complete Kinetis solutions for professional needs, training and support: http://www.utasker.com/kinetis.html
Kinetis KL02/KL03/KL05:
- http://www.utasker.com/kinetis/FRDM-KL02Z.html
- http://www.utasker.com/kinetis/FRDM-KL03Z.html
- http://www.utasker.com/kinetis/FRDM-KL05Z.html
uTasker: supporting >1'000 registered Kinetis users get products faster and cheaper to market
Request Free emergency remote desk-top consulting at http://www.utasker.com/services.html

Open Source version at https://github.com/uTasker/uTasker-Kinetis

0 件の賞賛
返信

2,485件の閲覧回数
tomazlov
Contributor II

Mark, I still think your answer in incorrect: settings logic '1' to NMI_DIS does enable NMI pin (as opposed to human understanding of the register flag name). More information can be found in:

https://community.nxp.com/message/498526?commentID=498526#comment-498526 (KL02_NMI.pdf)

https://www.nxp.com/docs/en/reference-manual/KL03P24M48SF0RM.pdf (Table 6-2. Flash Option Register (FTFA_FOPT) definition)

BR

0 件の賞賛
返信

2,485件の閲覧回数
mjbcswitzerland
Specialist V

Tomaz

You are right that I seem to have made a mistake in my statement since '1' enables the NMI pin and '0' disables it.
These are the definitions that I use:

      #define FTFL_FOPT_NMI_DISABLED      0x00
      #define FTFL_FOPT_NMI_ENABLED       0x04

Regards

Mark