I need help to solve my k64 issue, after boot loading the board, the red and green lights turns on at the same time so the board is inactive.
how I could solve this problem?
解決済! 解決策の投稿を見る。
Hello Mona,
Please do as :
(1)
Copy and past "JLink_OpenSDA_V2.bin:(please see the attachment ) to the BOOTLOADER drirve.
Unplug the USB cable and plug it in again.
(2) Find one demo code to test .
If still can not work , please send your project to me , i can test it on my side.
Hope it helps
Alice
Hello Mona, I am also facing the same issue I'm trying to use the solution Alice has provided but it seems like it's not working, could you please share any useful information regarding this problem if you have any, thank you
Thank you so much for your replies, I tried all your suggestions, but still no communication. I am using mbed compiler and also KDS. I have attached a picture of my board just to show you how the both lights are on.
Hello Mona,
Does D1 led light after you only plug the USB ?
If yes, i have check the Sch about the FRDM-K64 board , this is the rest led, maybe the board is broken.
And do you have other FRDM-K64 board ?
BR
Alice
I'm still not able to resolve my issue with this board and I really need your help to guide me to fix it.
Please if someone has an idea just forwarded it to me.
Thanks
Mona,
What software environment IDE (CW, KDS, etc) are you using to program your FRDM-K64 board? Are you using the OPENSDA or any external debug tool?
One suggestion is to try programming the Hello World demo from the Kinetis SDK 1.3.0 in Kinetis Design Studio and verify if that application is running.
Regards,
Johnny
P&E Microcomputer Systems
Hello Mona Khanafriboor:
Were you able to resolve your issue?
If not, could you please provide more details and the procedure you are following? This way we can provide better suggestions.
Regards!
Jorge Gonzalez
Hi Jorge and Alice
Thank you so much for your reply, Actually my issue did not solve yet even when I upload new application to it, the 2 red and green lights stayed on, these 2 lights are right cross the reset button. I'm not sure if the board needs any special fixing or it is totally damage.
Looking forward for your advises.
Mona
Hello Mona,
Please do as :
(1)
Copy and past "JLink_OpenSDA_V2.bin:(please see the attachment ) to the BOOTLOADER drirve.
Unplug the USB cable and plug it in again.
(2) Find one demo code to test .
If still can not work , please send your project to me , i can test it on my side.
Hope it helps
Alice
Hey Alice,
I actually went back to your advice and I follow your steps and now my board is functioning correctly.
Thank you so much.
My Best
Hello Mona,
I think it is no problem with your board , you can create a simple project to test it , for example only turn on the red lights.
Hope it helps
Alice