Missing k53_tower.h from KINETIS512_V2_SC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Missing k53_tower.h from KINETIS512_V2_SC

ソリューションへジャンプ
2,376件の閲覧回数
ClausStovgaard
Contributor III

Working with the Kinetis K53 devices I needed to use the Kinetis 100MHz Rev 2 Example Projects (Rev 1.0)

Direct link to KINETIS512_V2_SC.zip - Kinetis 100MHz Rev 2 Example Projects 

It contains k60_tower.h under src/platforms/k60_tower.h though as seen in src\common\common.h a file named k53_tower exsist for a K53 tower board. Can anyone provide a place where this is located? Looked into all the code snippets package I could find på have not seen it yet.

I would imagne the license for k53_tower is the same as k60_tower, but if anyone can confirm this, it would be great.

Kind regards

Claus

0 件の賞賛
返信
1 解決策
2,229件の閲覧回数
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Hello Claus,

Here are the examples, hope they work. 

This package is not available in the web page anymore because this codes are for previous silicon versions. the tower k53 was not redesigned for the new silicon version but the tower K60 was redesigned (the old is TWR-K60DN512 and the new is TWR-K60D100M).

have a great day.

best regards

Jonathan Iglesias 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,229件の閲覧回数
ClausStovgaard
Contributor III

Thanks for the answer.

0 件の賞賛
返信
2,230件の閲覧回数
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Hello Claus,

Here are the examples, hope they work. 

This package is not available in the web page anymore because this codes are for previous silicon versions. the tower k53 was not redesigned for the new silicon version but the tower K60 was redesigned (the old is TWR-K60DN512 and the new is TWR-K60D100M).

have a great day.

best regards

Jonathan Iglesias 

0 件の賞賛
返信