Microcontroller thickness 50um

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Microcontroller thickness 50um

1,389 次查看
kachen_chanthet
Contributor I

Hi, I'm looking for microcontroller in die form which is direct bonding, flip chip with bump  and has total thickness not over than 50um and die dimension 2x2mm (could be less or more), Could anyone how may concern please share your information to us.

0 项奖励
回复
1 回复

1,306 次查看
AldoG
NXP TechSupport
NXP TechSupport

Hello,

 

Please take a look to the MKL02Z32CAF4, which have

0.4 mm pitch; 1.94 mm x 1.99 mm x 0.6 mm body.

This is one of our tiniest MCUs.

 

Hope this helps,

Regards,
Aldo.

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复