Microcontroller thickness 50um

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Microcontroller thickness 50um

1,394件の閲覧回数
kachen_chanthet
Contributor I

Hi, I'm looking for microcontroller in die form which is direct bonding, flip chip with bump  and has total thickness not over than 50um and die dimension 2x2mm (could be less or more), Could anyone how may concern please share your information to us.

0 件の賞賛
返信
1 返信

1,311件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

 

Please take a look to the MKL02Z32CAF4, which have

0.4 mm pitch; 1.94 mm x 1.99 mm x 0.6 mm body.

This is one of our tiniest MCUs.

 

Hope this helps,

Regards,
Aldo.

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信