Micro C RTOS in Kinetics KV5 series

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Micro C RTOS in Kinetics KV5 series

2,236 Views
cronddaemon2
Contributor I

Hi All,

Am new to Kinetics.

I am planning to use Kinetics KV5 series [TWR-KV58F220M ], which is based on ARM-Cortex M7.

As per Micirium site, uc/OS-III supports Cortex M7 architecture. [µC/OS-III Kernel Port Availability  | Micrium ]

But, I dont see any official statement from NXP about the same.

So, I want to confirm whether, I can use Micrium RTOS III in TWR-KV58F220M or not ?

[ If the question does not belong to this forum,I request the moderator to move it, to corresponding place ]

Thanks

3 Replies

2,096 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello crond daemon:

I am currently checking about your question with the development team. Please let me reply as soon as I get some feedback.

Regards!

Jorge Gonzalez

2,096 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello crond daemon:

Just as heads up there is an upcoming KSDK release for KV5x which includes uC/OSII and uC/OSIII support. For the moment it is still under development/testing and unfortunately I don't have an estimate release time, but if I get any news I will let you know.

Regards!

Jorge Gonzalez

2,096 Views
cronddaemon2
Contributor I

Hello Jorge,

Thank you for the heads up . Really appreciate it. I will also look for the new release news.

0 Kudos
Reply