Mesh Network with BLE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Mesh Network with BLE

2,755 Views
notanivipul
Contributor II

HI 

I am using MKW-38 evaluation board for my project. It needs my evaluation board to be connected as slave to a master device via Bluetooth and also at the same time it needs to scan for nearby Bluetooth devices.

Does MKW-38 supports this and if yes, then please send me a link to documentation or an example code that I can refer for further development.

Thanks and regards,

Vipul

Labels (1)
0 Kudos
Reply
1 Reply

2,744 Views
nxf56274
NXP Employee
NXP Employee

Hi,

The example w_uart meet your demand. For detailed information, you can refer attachment ,chapter 5.18. It has two roles in one device.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply