Mesh Network with BLE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Mesh Network with BLE

2,694件の閲覧回数
notanivipul
Contributor II

HI 

I am using MKW-38 evaluation board for my project. It needs my evaluation board to be connected as slave to a master device via Bluetooth and also at the same time it needs to scan for nearby Bluetooth devices.

Does MKW-38 supports this and if yes, then please send me a link to documentation or an example code that I can refer for further development.

Thanks and regards,

Vipul

ラベル(1)
0 件の賞賛
返信
1 返信

2,683件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

The example w_uart meet your demand. For detailed information, you can refer attachment ,chapter 5.18. It has two roles in one device.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信