Memory to SPI (Peripheral) via DMA code snippet for KM34Z128

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Memory to SPI (Peripheral) via DMA code snippet for KM34Z128

903件の閲覧回数
phamsa
Contributor III
Hi Triggered by an external interrupt, I would like to send 64 bytes buffer (array) through SPI Bus using DMA, can I have any example for the same Target MCU : MKM34Z128 (50 Mhz) Thank you, Paddy
タグ(2)
0 件の賞賛
返信
1 返信

890件の閲覧回数
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @phamsa,

Unfortunately, this specific example that you mention is not available but in the SDK for the KM34 (75MHz) you can find an example using an SPI DMA transfer using a software trigger. The SDK is not straight compatible with the KM34 (50 MHz) but the SPI and DMA should be the same.

Best Regards,
Alexis Andalon

0 件の賞賛
返信