Memory to SPI (Peripheral) via DMA code snippet for KM34Z128

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Memory to SPI (Peripheral) via DMA code snippet for KM34Z128

892 次查看
phamsa
Contributor III
Hi Triggered by an external interrupt, I would like to send 64 bytes buffer (array) through SPI Bus using DMA, can I have any example for the same Target MCU : MKM34Z128 (50 Mhz) Thank you, Paddy
标记 (2)
0 项奖励
回复
1 回复

879 次查看
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @phamsa,

Unfortunately, this specific example that you mention is not available but in the SDK for the KM34 (75MHz) you can find an example using an SPI DMA transfer using a software trigger. The SDK is not straight compatible with the KM34 (50 MHz) but the SPI and DMA should be the same.

Best Regards,
Alexis Andalon

0 项奖励
回复