May I know how can I program a .axf file into MKL27z128VFT4?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

May I know how can I program a .axf file into MKL27z128VFT4?

3,223 次查看
ecang
Contributor I

I have an USB-Multilink Universal flash programmer and an AXF file.  Please advice how can I perform flash programming of .AXF file into NXP MKL27z128VFT4 ?

mkl27z #AXF file programming usb multilink universal    #flash programming‌

0 项奖励
回复
1 回复

1,189 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi EC ANG,

    Do you have the .axf project with IDE? If you use the IDE, it can downloaded the project with the Mutlilink.

    But if you want to download the .axf, .hex, .bin file with the PE multilink directly without the IDE, you need to use the P&E's  specific software:

PEmicro - P&E Microcomputer Systems: Over 30 years as an Industry leader in Embedded Systems Develop... 

    More details, you need to check it with the P&E engineer.

    If you use the IDE project, it will be very simple, you just need configure the debugger interface as P&E Multilink.

Wish it helps you!

If you still have question about it, please kindly let me know!

   

   


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复