MQX or EGUI needs

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MQX or EGUI needs

1,230件の閲覧回数
ankurchauhan
Contributor I

Hi,

I Want to know what the need of eGui.

In my project I have to use LCD via EBI interface(using k70). Is this software required for that.

Currently I'm using bareboard project..

Regards

Ankur

ラベル(1)
0 件の賞賛
返信
1 返信

1,150件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hello,

The K70 integrates the LCDC module to connect and manage the LCD. You don't need MQX (RTOS) for using eGUI (graphic library), you can also use bare metal approach with eGUI. Using MQX will help in the case you need USB, TCP/IP, file system, etc… apart from the graphic user interface. In that case, for example MQX + MFS (file system) allows you to store graphic resources in external USB, SD card, etc…

I hope this helps.

Luis

0 件の賞賛
返信