MQX or EGUI needs

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MQX or EGUI needs

1,240 次查看
ankurchauhan
Contributor I

Hi,

I Want to know what the need of eGui.

In my project I have to use LCD via EBI interface(using k70). Is this software required for that.

Currently I'm using bareboard project..

Regards

Ankur

标签 (1)
0 项奖励
回复
1 回复

1,160 次查看
LuisCasado
NXP Employee
NXP Employee

Hello,

The K70 integrates the LCDC module to connect and manage the LCD. You don't need MQX (RTOS) for using eGUI (graphic library), you can also use bare metal approach with eGUI. Using MQX will help in the case you need USB, TCP/IP, file system, etc… apart from the graphic user interface. In that case, for example MQX + MFS (file system) allows you to store graphic resources in external USB, SD card, etc…

I hope this helps.

Luis

0 项奖励
回复