MKW41Z

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MKW41Z

1,419 Views
sheshnathchauha
Contributor II

Hi all,

I am trying to interface a display using spi1 with MKW41Z Devlopment board.And it work at normal run mode properly but when i am trying it to run at very low power mode then it display very very slow(take about 19sec).so please give me suggetion for display within 3s in very low mode using spi1

Tags (1)
0 Kudos
Reply
1 Reply

1,268 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

When you are in Very Low Power Mode there are some restrictions in core/systems clocks which are described in chapter 5.5.2 VLPR mode clocking. The clock dividers cannot be changed while in VLPR mode for which you have to set them up prior to entering VLPR mode. These new values affect the module baud rate and clock delay generation (chapter 36.4.3).

Reference manual:

http://cache.nxp.com/assets/documents/data/en/reference-manuals/MKW41Z512RM.pdf?fsrch=1&sr=2&pageNum...

Regards,

Ivan.

0 Kudos
Reply