MKW30Z framework LED.h LED.c limitations

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MKW30Z framework LED.h LED.c limitations

763件の閲覧回数
lucianfiran
Contributor V

KW40Z_Connectivity_Software_1.0.1 KSDK_1.3.0 IAR 7.5

It seems rather complicated to insert led support for the 5 th led or the n th led.

I think the mapping is the issue here:
/*
* LEDs mapping
*/
#define LED1                     0x01
#define LED2                     0x02
#define LED3                     0x04
#define LED4                     0x08
#define LED_ALL                  0x0F
#define LED1_FLASH               0x10
#define LED2_FLASH               0x20
#define LED3_FLASH               0x40
#define LED4_FLASH               0x80
#define LED_FLASH_ALL            0xF0  /* flash all LEDs */

like going on 16bit (0x0100) ?

Is there a easy-er way ?

Another limitation I think is missing a polarity software switch like
normal/inverted output.


To fully disable led support:

/* Enable/Disable LED supoort */
#define  gLEDSupported_d                TRUE
/* Specifies the number of physical LEDs on the target board */
#define gLEDsOnTargetBoardCnt_c 4

It is  enough to switch gLEDSupported_d FALSE  ?

or more ?

Thank you,
Lucian

ラベル(1)
0 件の賞賛
返信
0 返答(返信)