MKV44 SDK 2.8.0 missing XBARA Driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MKV44 SDK 2.8.0 missing XBARA Driver

Jump to solution
2,881 Views
katha
Contributor II

Hello,

I try to add the XBARA driver to my MKV44 project, but I cant find it in the SDK. In SDK for MK64 2.8.2 it is available. Is there any reason?

Thanks a lot and kind regards

0 Kudos
Reply
1 Solution
2,871 Views
Masmiseim
Senior Contributor I

I can not explain why they are missing for the KV44, however they are included in the SDK package for the KV46. This should also work for the KV44. I would give it a try

View solution in original post

0 Kudos
Reply
2 Replies
2,872 Views
Masmiseim
Senior Contributor I

I can not explain why they are missing for the KV44, however they are included in the SDK package for the KV46. This should also work for the KV44. I would give it a try

0 Kudos
Reply
2,848 Views
katha
Contributor II

Is there a possibility to add it soon?

Whats about the ftm driver? In reference manual it has an extra section besides the eFlexPWM

Regards

0 Kudos
Reply