MKL27Z64VLH4 replacement

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MKL27Z64VLH4 replacement

2,123 Views
dusek_martin
Contributor IV

Hi,

is there a replacement for MKL27Z64VLH4, which is not in stock?

I need LQFP64, crystalless USB operation (48 MHz internal clock), min 64 kB flash, pin compatibility for power, USB, SWD and analog power/reference. On our board, all MKL27 pins are used, however, no specific function on pins is needed (just GPIO).

Thanks, Martin

Tags (1)
0 Kudos
Reply
3 Replies

2,114 Views
bobpaddock
Senior Contributor IV

Some K32L's will cross to the 27 at the pin level. 
Software is not drop in compatible.

Like most everything from most everyone those are not available either.




0 Kudos
Reply

2,102 Views
dusek_martin
Contributor IV

Can you please give me exact part number? I listed all K32L's with LQFP64 package but unfortunately all 5 parts I got have VOUT33 and VREGIN pins (K27 has USB_VDD pin). This is not compatible with our board.

Tags (1)
0 Kudos
Reply

2,099 Views
bobpaddock
Senior Contributor IV

KL to K32L migration guide:

https://www.nxp.com/docs/en/application-note/AN12779.pdf

As I said some of the K32Ls cross, you may have one that doesn't..



0 Kudos
Reply