MKL27Z64VLH4 replacement

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MKL27Z64VLH4 replacement

2,128 次查看
dusek_martin
Contributor IV

Hi,

is there a replacement for MKL27Z64VLH4, which is not in stock?

I need LQFP64, crystalless USB operation (48 MHz internal clock), min 64 kB flash, pin compatibility for power, USB, SWD and analog power/reference. On our board, all MKL27 pins are used, however, no specific function on pins is needed (just GPIO).

Thanks, Martin

标记 (1)
0 项奖励
回复
3 回复数

2,119 次查看
bobpaddock
Senior Contributor IV

Some K32L's will cross to the 27 at the pin level. 
Software is not drop in compatible.

Like most everything from most everyone those are not available either.




0 项奖励
回复

2,107 次查看
dusek_martin
Contributor IV

Can you please give me exact part number? I listed all K32L's with LQFP64 package but unfortunately all 5 parts I got have VOUT33 and VREGIN pins (K27 has USB_VDD pin). This is not compatible with our board.

标记 (1)
0 项奖励
回复

2,104 次查看
bobpaddock
Senior Contributor IV

KL to K32L migration guide:

https://www.nxp.com/docs/en/application-note/AN12779.pdf

As I said some of the K32Ls cross, you may have one that doesn't..



0 项奖励
回复