MKL25Z128 NOR Flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MKL25Z128 NOR Flash

1,454件の閲覧回数
mallapuramphani
Contributor I

Hello,

I want to interface NOR flash, with MKL25Z128 on SPI mode.

My query is how much maximum/minimum Memory i can do. 

Thanks & regards

Phani

タグ(1)
0 件の賞賛
返信
1 返信

1,378件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Using the SPI mode to connect external SPI Flash, there doesn't with the memory size limitation.

The external SPI Flash memory doesn't add to the KL25 memory map.

Thank you for the attention.


Have a great day,
Mike

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信