MKL25Z128 NOR Flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MKL25Z128 NOR Flash

1,449 Views
mallapuramphani
Contributor I

Hello,

I want to interface NOR flash, with MKL25Z128 on SPI mode.

My query is how much maximum/minimum Memory i can do. 

Thanks & regards

Phani

Tags (1)
0 Kudos
Reply
1 Reply

1,373 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Using the SPI mode to connect external SPI Flash, there doesn't with the memory size limitation.

The external SPI Flash memory doesn't add to the KL25 memory map.

Thank you for the attention.


Have a great day,
Mike

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply