MKL25Z - Fresh device programming via USB port

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MKL25Z - Fresh device programming via USB port

ソリューションへジャンプ
2,121件の閲覧回数
lore
Contributor I

Hello everyone,

Is it possible to flash a bootloader into a fresh new MKL25Z128VLK4 mcu via USB port (without using SWD/JTAG port)? Or I do need to breakout JTAG pins to my custom KL25 board, and buy an external programmer?

My goal is to to set up by custom board as Mass Storage Device so that new binaries can be copied on it, just like the FRDM behavior.

Thanks in advance

Lore

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 解決策
1,903件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Lore,

the KL25Z has no ROM bootloader (newer Kinetis devices do have this). So you have to use the SWD/JTAG port to program it the first time.

I hope this helps,

Erich

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,904件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Lore,

the KL25Z has no ROM bootloader (newer Kinetis devices do have this). So you have to use the SWD/JTAG port to program it the first time.

I hope this helps,

Erich

0 件の賞賛
返信
1,903件の閲覧回数
lore
Contributor I

Hi Erich,

Thanks for your answer, I think you are referring to the supported device table in the KBOOT page. In this case KL27 should be the right choice.

Lore

0 件の賞賛
返信