MKL02Z32VFK4 pinout - central PAD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MKL02Z32VFK4 pinout - central PAD

ソリューションへジャンプ
3,366件の閲覧回数
lucaag
Contributor III

HW DESIGN:

The QFN-24 case provides a central PAD, which is probably used for thermal reasons. I was not able to find where this PAD should be connected: should it be connected to GND or should it be left unconnected?

Thank you in advance, Luca

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
3,217件の閲覧回数
mjbcswitzerland
Specialist V

Hi

This question has been asked many times and there are many responses at the forum too. Eg. one from 5 years ago: https://community.nxp.com/message/317841 

I suppose the answer is the same for all Kinetis parts and I never understood why this is not documented in the data sheet, which would save many engineers worrying about getting it wrong.....

Regards

Mark

元の投稿で解決策を見る

5 返答(返信)
3,218件の閲覧回数
mjbcswitzerland
Specialist V

Hi

This question has been asked many times and there are many responses at the forum too. Eg. one from 5 years ago: https://community.nxp.com/message/317841 

I suppose the answer is the same for all Kinetis parts and I never understood why this is not documented in the data sheet, which would save many engineers worrying about getting it wrong.....

Regards

Mark

3,217件の閲覧回数
lucaag
Contributor III

Yes, it seems it's not well documented.

May be I've not read the documents so carefully, but I was not able to find any indication. An upgrade by NXP would be appreciated. 

Thank you very much,

Luca

0 件の賞賛
返信
3,217件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

The recommendation is connected to ground, please check AN2467 Power quad flat no-lead (PQFN) package.

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,217件の閲覧回数
lucaag
Contributor III

Hello Robin.

Sorry, I don't see your answer (may be you linked something, but it's not visible in the message).

Could you check?

Thank you in advance,

Luca

0 件の賞賛
返信
3,217件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Sorry!

I have fixed the reply.