Kinetis KL1x and KL2x thermal/exposed PAD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis KL1x and KL2x thermal/exposed PAD

Jump to solution
2,465 Views
lfschrickte
Contributor IV

Hi,

I can't find in the Kinetis family documentation any reference to the thermal pad connection! Is it isolated? Can I connect it to ground? Both alternatives are right?

I know it is usual to connect it to ground, but as a designer I prefer to see it written by freescale in order to be sure I can connect it. The only reference I've saw is the crystal layout guidelines in the Product Quick reference in which the Thermal Pad is connected to the ground.

Does anyone knows this information for sure? If it is written somewhere I've missed, please point me out!

Thank you

Labels (1)
1 Solution
2,157 Views
Pepe_Ruiz
Contributor IV

Hi Luis Fernando,

The thermal pad is isolated just like you said and the recomendation is to ground it.

just be carefull with the solder

regards

/Jose

View solution in original post

0 Kudos
Reply
2 Replies
2,158 Views
Pepe_Ruiz
Contributor IV

Hi Luis Fernando,

The thermal pad is isolated just like you said and the recomendation is to ground it.

just be carefull with the solder

regards

/Jose

0 Kudos
Reply
2,157 Views
lfschrickte
Contributor IV

Thank you Jose!

I wish this information was present in the Datasheet or the Reference

Manual. Even if it is something quite "obvious", it is always nice to have

it confirmed somewhere!

I appreciate your help.

Luiz Fernando

Luiz Fernando Schrickte