MKL02Z32VFK4 pinout - central PAD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MKL02Z32VFK4 pinout - central PAD

Jump to solution
827 Views
lucaag
Contributor III

HW DESIGN:

The QFN-24 case provides a central PAD, which is probably used for thermal reasons. I was not able to find where this PAD should be connected: should it be connected to GND or should it be left unconnected?

Thank you in advance, Luca

Labels (1)
Tags (1)
0 Kudos
1 Solution
678 Views
mjbcswitzerland
Specialist V

Hi

This question has been asked many times and there are many responses at the forum too. Eg. one from 5 years ago: https://community.nxp.com/message/317841 

I suppose the answer is the same for all Kinetis parts and I never understood why this is not documented in the data sheet, which would save many engineers worrying about getting it wrong.....

Regards

Mark

View solution in original post

5 Replies
679 Views
mjbcswitzerland
Specialist V

Hi

This question has been asked many times and there are many responses at the forum too. Eg. one from 5 years ago: https://community.nxp.com/message/317841 

I suppose the answer is the same for all Kinetis parts and I never understood why this is not documented in the data sheet, which would save many engineers worrying about getting it wrong.....

Regards

Mark

678 Views
lucaag
Contributor III

Yes, it seems it's not well documented.

May be I've not read the documents so carefully, but I was not able to find any indication. An upgrade by NXP would be appreciated. 

Thank you very much,

Luca

0 Kudos
678 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

The recommendation is connected to ground, please check AN2467 Power quad flat no-lead (PQFN) package.

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
678 Views
lucaag
Contributor III

Hello Robin.

Sorry, I don't see your answer (may be you linked something, but it's not visible in the message).

Could you check?

Thank you in advance,

Luca

0 Kudos
678 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Sorry!

I have fixed the reply.