MKL02Z32CAF4R

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,043件の閲覧回数
sebastianmartiu
Contributor I

I have two questions about the Kinetis MKL02Z32CAF4R:

Is the Kinetis MKL02Z32CAF4R with the WLCSP case (Pitch 0.4mm) still in production?

Could I use the Kinetis MKL02Z32CAF4R without a external XTAL crystal?

0 件の賞賛
返信
1 解決策
1,966件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

The Kinetis MKL02Z32CAF4R with the WLCSP case (Pitch 0.4mm) still in production(Active).

Status.png

Yes. You can use internal reference clock.

IRC.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
1,967件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

The Kinetis MKL02Z32CAF4R with the WLCSP case (Pitch 0.4mm) still in production(Active).

Status.png

Yes. You can use internal reference clock.

IRC.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,966件の閲覧回数
sebastianmartiu
Contributor I

Thank you Shen :-)

0 件の賞賛
返信