MKL02Z32CAF4R

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MKL02Z32CAF4R

Jump to solution
2,123 Views
sebastianmartiu
Contributor I

I have two questions about the Kinetis MKL02Z32CAF4R:

Is the Kinetis MKL02Z32CAF4R with the WLCSP case (Pitch 0.4mm) still in production?

Could I use the Kinetis MKL02Z32CAF4R without a external XTAL crystal?

0 Kudos
Reply
1 Solution
2,046 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

The Kinetis MKL02Z32CAF4R with the WLCSP case (Pitch 0.4mm) still in production(Active).

Status.png

Yes. You can use internal reference clock.

IRC.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
2,047 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

The Kinetis MKL02Z32CAF4R with the WLCSP case (Pitch 0.4mm) still in production(Active).

Status.png

Yes. You can use internal reference clock.

IRC.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,046 Views
sebastianmartiu
Contributor I

Thank you Shen :-)

0 Kudos
Reply