MKE15 Stop Mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MKE15 Stop Mode

1,662件の閲覧回数
David_94
Contributor I

Hi,

I'm trying to make the MKE15 enter STOP mode. I found this code on the forum

void stop (void)
{
 /* Set the SLEEPDEEP bit to enable deep sleep mode (STOP) */
 SCB->SCR |= SCB_SCR_SLEEPDEEP_Msk; 

 /* WFI instruction will start entry into STOP mode */
#ifndef KEIL
        // If not using KEIL's uVision use the standard assembly command
 asm("WFI");
#else
        // If using KEIL's uVision, use the CMSIS intrinsic
 __wfi();
#endif
}

Is it enough?

How do I have to set registers in order that the micro wake up from stop mode if I have an active edge on the UART?

0 件の賞賛
返信
2 返答(返信)

1,638件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

We have the example about power manage in directory '2.9.0_FRDM-KE15Z\boards\frdmke15z\demo_apps\power_mode_switch'.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

1,647件の閲覧回数
mjbcswitzerland
Specialist V

Hi

STOP mode is controlled by the Cortex core so doesn't need any more registers configured (the various low leakage modes require additional setup).

STOP mode will exit whenever there is a pending interrupt so any peripheral (whose clock is not stopped in STOP mode) configured with an interrupt is adequate.

The asynchronous UART rx edge wake up is not needed in STOP mode - it is only needed in VLPS.

Regards

Mark
[uTasker project developer for Kinetis and i.MX RT]
Contact me by personal message or on the uTasker web site to discuss professional training, solutions to problems or rapid product development requirements

For professionals searching for faster, problem-free Kinetis and i.MX RT 10xx developments the uTasker project holds the key: https://www.utasker.com/kinetis/FRDM-KE15Z.html

0 件の賞賛
返信