does the Kinetis K81 USB suspend is available when connected with Android device?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

does the Kinetis K81 USB suspend is available when connected with Android device?

1,790 次查看
robinliao
Contributor I

Hello NXP

Is the usb pause mode available when connected to an Android phone/tablet?

I have implemented the USB suspend function on our device and it works fine

my usb devices can be suspended/resume when connected to the host PC

but when I connect to the Android phone, the usb device is always running, and will not enter the USB suspend state

How to configure the usb library to support usb suspend on Android devices? Or is this problem based on the Android configuration?

 

Thanks

Robin

0 项奖励
回复
2 回复数

1,745 次查看
robinliao
Contributor I

it looks like USB autosuspend did not enabled on the Android device?

thank you for your response

0 项奖励
回复

1,757 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi Robin,

We do not have specific configuration for Android devices in our USB stack, therefore, I think the problem could be on the Android side, maybe there is a some driver missing.

Best regards,

Felipe