MKE04Z8VFK4 Pin configuration in MCUXpresso

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MKE04Z8VFK4 Pin configuration in MCUXpresso

ソリューションへジャンプ
1,220件の閲覧回数
chicagomike
Contributor III

Hi,

I'm developing for the MKE04Z8VFK4 on custom target hardware using MCUXpresso v11.6.1 on a Windows 10 box.

My latest problem is that I am unable to configure GPIOB and GPIOC pins using the pin configuration tool. When I add a row for a PTBx pin and click on the Peripheral cell, the drop menu only contains GPIOA. I also tried just typing in GPIOB or GPIOC but the tool doesn't allow that.

(See screenshot below)

How can I configure PTBx and PTCx pins with this tool?

Thanks,

Mike

no_other_gpio_ports.jpg

 

0 件の賞賛
返信
1 解決策
1,212件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Mike,

Sorry that the names of GPIO registers and port pin registers of KE series may confuse you in MCUXpresso IDE.

Please refer to the example of toggle PTB3 on FRDM-KE04Z:

PTB3 FRDM-KE04Z.pngfrdmke04z_hello_world toggle PTB3.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,213件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Mike,

Sorry that the names of GPIO registers and port pin registers of KE series may confuse you in MCUXpresso IDE.

Please refer to the example of toggle PTB3 on FRDM-KE04Z:

PTB3 FRDM-KE04Z.pngfrdmke04z_hello_world toggle PTB3.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
1,189件の閲覧回数
chicagomike
Contributor III

Thanks again, Robin for your patient support!

The 'A' at the end of the peripheral name was the confusing factor for me, but now I'm back on track.

Mike

0 件の賞賛
返信