MKE04Z128VLK4 SPI Fan-out

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MKE04Z128VLK4 SPI Fan-out

2,087 Views
bon
Contributor I

What is the fanout of MKE04Z128VLK4 SPI port?

How many slaves can be connected to the SPI port?

I would like to connect 8 slaves to the SPI port.

Best regards,

#MKE04Z128VLK4

Tags (1)
0 Kudos
Reply
3 Replies

1,955 Views
bon
Contributor I

Dear Daniel,

Thank you for your reply.

I would like to connect 8 slaves to one SPI port.

I'm worried about fan out by connecting 8 slaves to one port.

A circuit diagram is attached.

The CS pin is simulated with GPIO.

Best regards,

Ryutaro

新規 Microsoft PowerPoint プレゼンテーション.png

0 Kudos
Reply

1,955 Views
danielchen
NXP TechSupport
NXP TechSupport

It is OK to connect 8 slaves to one SPI port.

Regards

Daniel

0 Kudos
Reply

1,955 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Ryutaro:

MKE04Z128VLK4 contains two SPI modules that support 8-bit data length.

For the limited pin source, only can connect 2 slaves.  If you need to support 8 slaves, you need to use GPIO to simulate CS.

Regards

Daniel

0 Kudos
Reply