MKE04Z IC DEBUG KWIKSTIK SWD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MKE04Z IC DEBUG KWIKSTIK SWD

1,421 Views
alexloban
Contributor II

Dear Kinetis Community,

im very new in embedded system. And have now a first problem. 

Im buy me Kinetis MKE04Z8VTG4 chips in TSSOP 16 package and place one on a pcb.

Buy me SWD Cable, Connector adapter to DIP. 

And Kwikstik SWD connecter (J8).

All parts are placed.

In Kwikstik manual i have read i can debug via J8 connector all Kinetis IC's.

I connect Kwikstik and MKE04Z, start J-Link flash and try to erase chip. and get error,

can not connect. 

HOW I CAN COUNT PINS of SWD connector wich direction  ? FROM LEFT TO RIGHT  ? UP AND DOWN ??

9-0 Kopie.jpg

DATASHEET KWIKSTIK DEBUG SWD

Screen Shot 2018-06-08 at 06.18.22.png

DATASHEET MKE04Z  BUT I DONT  SEE A POINT OF PIN COUNTING ON THE CHIP I SEE A ROUND MARK LIKE IMAGE DOWN.

PIN MAPPING

Screen Shot 2018-06-08 at 06.11.55.png

Screen Shot 2018-06-08 at 06.12.47.png

MY CONNECTION.

tssopA.jpg

  

It was my first experience. And im sure i do something wrong or its no possible do flash or debug with kwikstik.

I have direct cables to the pins without capacitor, resistors. 

Can you help me ?

If it no possible to debug, pleas tell me a little bit what i need to flash chip. i will start a project with out dev board :smileyhappy: only PCB. 

THANK YOU VERY MUCH !

alex#

0 Kudos
Reply
1 Reply

1,230 Views
adamsojecki
Contributor I

ConnNub.jpg

Here's the correct numbering of the pins SWD connector on KwikStik.

Good luck,

Adam.

0 Kudos
Reply