Do Freedom boards arrive with Arduino connectors pre-installed or not ? On both sides?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Do Freedom boards arrive with Arduino connectors pre-installed or not ? On both sides?

ソリューションへジャンプ
1,494件の閲覧回数
Anonymous
適用対象外

I want to order FRDM-K64F but it is not clear if it comes with connectors already installed. The user manual shows female Arduino sockets on the top layer, not clear whether there are male connectors on the other side. I need connectors on the bottom side to connect this board to my motherboard. Is it possible to order this board without connectors installed? Or are there male connectors on the bottom side by default?

Please let me know.

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 解決策
1,403件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

No, FRDM-K64F doesn't have mail Arduino connectors on the bottom side, and yes, the female Arduino sockets on the top layer are pre-installed by default. You have to change the connectors manually. Sorry for the inconvenience that might cause.


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,404件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

No, FRDM-K64F doesn't have mail Arduino connectors on the bottom side, and yes, the female Arduino sockets on the top layer are pre-installed by default. You have to change the connectors manually. Sorry for the inconvenience that might cause.


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信