MK66FN2M0VMD18 digital 5v input tolerant

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MK66FN2M0VMD18 digital 5v input tolerant

ソリューションへジャンプ
4,275件の閲覧回数
henrynguyen
Contributor IV

Hello,

we have used the  MK61FN1M0VMD12  part in the past and its spec said very clearly that all digital IO pins are 5V input tolerant.  see attachment for MK61 snap shot.

now, we are looking at MK66FN2M0VMD18 device but can not find any 5v input tolerant on the data sheet.  we are surprised because the MK61F and MK66F should be the same family.

can you please clarify?  This is very confusing on why the same family part does not have the same 5v input tolerant.

Thanks and Best Regards,

Henry Nguyen

0 件の賞賛
返信
1 解決策
4,199件の閲覧回数
nxf77486
NXP TechSupport
NXP TechSupport

Hello @henrynguyen ,

 

The assumptions are correct all the Kinetis pins, with exception of the specified have an input mode of 5V tolerant.

We will review out documentation in order to updated.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
4,200件の閲覧回数
nxf77486
NXP TechSupport
NXP TechSupport

Hello @henrynguyen ,

 

The assumptions are correct all the Kinetis pins, with exception of the specified have an input mode of 5V tolerant.

We will review out documentation in order to updated.

0 件の賞賛
返信
4,264件の閲覧回数
myke_predko
Senior Contributor III

Hi @henrynguyen 

What you're showing is exactly right, all the Kinetis pins, with the exception of the specified ones, in input mode are 5V tolerant.  I recommend a 1k resistor between the 5V output to the Kinetis input pin to minimize any potential current flow from the output into the Kinetis.  

We had a discussion on using the pins as Open Collector outputs and you can see it here:  5v Tolerant pins as Open Collector Drivers). 

Good luck!

0 件の賞賛
返信
4,258件の閲覧回数
henrynguyen
Contributor IV

Hi Myke_predko

thank you so much for your input.  
However I am still uneasy because I am not sure why NXP did not spell this out explicitly for K66F data sheet.  
In our application, the RXD pin from CAN transceiver drives a digital 5v to the K66F input.  The current is low but it is 5v and the K66F VDD is 3.3v.  

can someone from NXP please confirm if our assumptions are right and the data sheet will be updated to reflect this?

thanks

Henry