MK64FX512 : VREF_OUT voltage drift

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MK64FX512 : VREF_OUT voltage drift

ソリューションへジャンプ
1,692件の閲覧回数
koichisakagami
Contributor II

Dear community,

We consider the VREF_OUT voltage drift.

In DataSheet Table 36. VREF full-range operating behaviors ,
It is described that VOUT = 1.198 V (max);( Vout Voltage reference output with factory trim at nominal VDDA and temperature= 25 °C ) .

  Vtdrift = 15mV ( max ) ;(Vmax -Vmin across the full temperature range)
  Vvdrift = 2mV ( max );(Vmax -Vmin across the full voltage range)

Next,
Table 38. VREF limited-range operating behaviors ,
It is described that VOUT = 1.225 V (max);temperature= 0 ~ 50 °C

We calculated a max case value for voltage drift.
1.198 + 0.015 + 0.002 = 1.215

[Question]
Why  is the max case value ( we  calculated) smaller than Table 38 value ?
1.215 < 1.225

Best Regards,
Koichi Sakagami

ラベル(1)
0 件の賞賛
返信
1 解決策
1,531件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Koichi,

It seems that there is discrepancy as you said. I seems that  that the Vtdrift spec has issue, some data sheet says that the maximum of Vtdrift is 80mV instead of 15mV. You can download the data sheet of the other Kinetis K family.

BR

Xiangjun Rong

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,532件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Koichi,

It seems that there is discrepancy as you said. I seems that  that the Vtdrift spec has issue, some data sheet says that the maximum of Vtdrift is 80mV instead of 15mV. You can download the data sheet of the other Kinetis K family.

BR

Xiangjun Rong

0 件の賞賛
返信